- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- Tutorials
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Accordion style
Style for accordions
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Border color | BorderColor | Color of the polygon border | |
Border width | BorderWidth | Thickness of the object border | |
Radius | Radius | Radius of the angles of the objects | |
Header background color | HeaderBackgroundColor | Background color for the header | |
Content background color | ContentBackgroundColor | Background color of the content | |
Header icon position | HeaderIconPosition | Position of the header icon |
Provide Feedback