- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- Tutorials
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Delete an event logger
Delete an event logger by removing the event logger object in
Project view
.
TIP:
You can disable an event logger without the need to completely remove the logger from the project. For more information, see Edit an event logger.
- InProject view, right-click an event logger object and selectDelete.
Provide Feedback