- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- Tutorials
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
ResourceURI.FromProjectRelativePath(path)
Returns a C# object of the
ResourceURI
type, with the URIType
of ProjectRelative
and that contains a relative path to a file than the ProjectFiles
folder.static ResourceUri FromProjectRelativePath(stringpath);
Arguments
- path(string)
- A relative path of a file in relation to theProjectFilesfolder.
Returns
- ResourceURI
- A C# object that contains the path indicated in the argument.
Example
The following example shows an API that returns a C#
projectRelativeResourceURI
object of the ResourceURI
type that contains the relative path Text1.txt
. The object is used as an argument of the .NET WriteAllText
API to create a Text1.txt
text file inside the ProjectFiles
folder.
var projectRelativeResourceUri = ResourceUri.FromProjectRelativePath("Text1.txt"); Log.Info(projectRelativeResourceUri.ProjectRelativePath); File.WriteAllText(projectRelativeResourceUri.Uri, "Hello world!");
Provide Feedback