- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- Tutorials
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Tag event
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Tag | Tag | ||
Index | Index | ||
Operation code | OperationCode | ||
Operation ID | OperationId | (Inherited from Driver event) | |
Transaction ID | TransactionIds | (Inherited from Driver event) | |
Timestamp | Timestamp | (Inherited from Driver event) | |
EventId | (Inherited from BaseEventType) | ||
EventType | (Inherited from BaseEventType) | ||
SourceNode | (Inherited from BaseEventType) | ||
SourceName | (Inherited from BaseEventType) | ||
Time | (Inherited from BaseEventType) | ||
ReceiveTime | (Inherited from BaseEventType) | ||
LocalTime | (Inherited from BaseEventType) | ||
Message | (Inherited from BaseEventType) | ||
Severity | (Inherited from BaseEventType) | ||
ConditionClassId | (Inherited from BaseEventType) | ||
ConditionClassName | (Inherited from BaseEventType) | ||
ConditionSubClassId | (Inherited from BaseEventType) | ||
ConditionSubClassName | (Inherited from BaseEventType) |
Provide Feedback