- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- Tutorials
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Access project nodes
You can access C# object members, OPC UA nodes, NetLogic objects, and session aliases.
C# object members
In C#, each property or method contained in an object is generically defined as a member of the object. The matching project node
BrowseName
identifies each member.
TIP:
To display the
BrowseName
of a property, hover over its name in the Property
pane. A tooltip appears with the BrowseName
, data type, and short description (if present).To access the members in hierarchical order, use the point.
In the following example, The
Acceleration
property of the Motor
object is set to the value of 123
.
Motor.Acceleration = 123;
In the following example, the value of the
Motor
object Speed
property is assigned to the value of the currentSpeed
C# integer variable.
int currentSpeed = Motor.Speed;
Project OPC UA nodes
To access a node in the C# information model, the node must be represented in the NetLogic by a matching C# object. To obtain the matching C# object, you can use these APIs:
To refer to the OPC UA nodes of the properties of a typed node, the name of the matching C# property consists of the
BrowseName
of the property to which the suffix is added. The following example shows a dynamic link set on theVariable
Text
property of a label through the API, accessing the property node represented by TextVariable
.
Label1.TextVariable.SetDynamicLink(speedValue);
Provide Feedback