OMRON EtherNet/IP driver
Observe these guidelines when working with the OMRON EtherNet/IP driver.
Supported controllers
The driver may support these controller families:
- OMRON® NJ Series
- OMRON® NX Series
- OMRON® NU Series
IMPORTANT:
The driver has been tested with NJ301-1100 firmware revision 1.09 and NJ101-9000 firmware revision 1.50.
Controller tags import
You can only import tags from
TXT
files in the offline mode.
IMPORTANT:
Before importing tags:
- In Sysmac® Studio, setNetwork PublishtoPublish only.
- From Sysmac® Studio, export tags to aTXTfile.
For more information, refer to the product documentation.
Data types
The driver supports these data types:
Controller data type | FactoryTalk Optix data type | Length | Notes |
|---|---|---|---|
BOOL | BOOL | 1 BIT | |
BYTE | BYTE | 1 BYTE | |
WORD | UINT16 | 2 BYTES | |
DWORD | UINT32 | 4 BYTES | |
LWORD | UINT64 | 8 BYTES | |
SINT | SBYTE | 1 BYTES | |
INT | INT16 | 2 BYTES | |
DINT | INT32 | 2 BYTES | |
USINT | BYTE | 1 BYTE | |
UINT | UINT16 | 2 BYTES | |
UDINT | UINT32 | 4 BYTES | |
LINT | INT64 | 4 BYTES | |
ULINT | UINT64 | 8 BYTES | |
REAL | FLOAT | 4 BYTES | |
LREAL | DOUBLE | 8 BYTES | |
TIME | DURATION | 4 BYTES | |
DATE | DATE TIME | 2 BYTES | Use these data types with Date and time objects, which allow you to set and view date and time data. |
TIME_OF_DAY(TOD) | UTC TIME | 4 BYTES | |
DATE_AND_TIME(DT) | DATE TIME | 8 BYTES | |
STRING(256) | STRING-MAX256 | 256 BYTES | |
ARRAY 1 dimensional | Type [dimension] | ||
ARRAY 2 dimensional | Type [1st dimension, 2nd dimension] | ||
ARRAY 3 dimensional | Type [1st dimension ,2nd dimension, 3rd dimension] |
Provide Feedback