Add Site

After adding the Region, the user needs to add the Site.
NOTE:
The following points are required to view data on
Site level dashboard
:
  • Data from different meters which are directly connected to a Site node will be considered for the data aggregation.
  • For consumption and demand charts, the respective resource meter has to be configured with the proper tag mapping.
  • For Cost charts, the respective rate schedule should be configured at the Site level.
  • For Emission, the respective emission factor should be configured at the Site level.
  • For Production and energy intensity charts should have correct tag mapping for production count measurement.
  • Harmonized units are defined at the Enterprise level and will be used to display harmonized consumption, intensity, or emissions data.
Perform the following steps to add a Site under Region:
  1. Select the
    Region
    from the hierarchy list.
  2. Click the [] icon and click
    Add
    .
    The
    Add New
    dialog is displayed.
    Add New Site Dialog
  3. Click
    Add
    .
    The
    Add Component
    dialog box is displayed.
    Add Component -Site Dialog
  4. Under
    Node
    , click
    Site
    and set these parameters:
    • Name
      : Provide a Site name.
    • Geolocation
      : Provide a latitude and longitude details of the Site.
      NOTE:
      After providing the values, use the up-arrow and down-arrow to increase and decrease the values.
    • Time zone
      : Select a time zone from the drop-down list.
    • Currency
      : Select a currency from the drop-down list.
    • Description
      : Provide a description of the Site.
    NOTE:
    In the Site component, the user can configure base details (geolocation, currency, time zone) and configure the Site level: Configure Resource Types, Site level: Configure Emissions Factors, Site level: Configure Measurands, Site level: Configure Parameters, and Site level: Configure Rate Schedules.
  5. Click
    Add
    .
The "
Site added under Region successfully
" message is displayed.
The user can also export the data file to local. For more details, see Export Data File.
Related Information
:
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal