Copy and Paste Component

Perform the following steps to copy and paste the component in the hierarchy list:
  1. Select the required component.
  2. Click the [] icon and click
    Copy
    .
    NOTE:
    If the user copies the parent component directly, they need to select
    with child
    or
    without child
    radio button in the
    Copy Component
    dialog and click
    Copy
    .
    Copy Component
    The "
    Component copied successfully
    " message is displayed.
  3. Select the required hierarchy component to paste the copied component.
  4. Click the [] icon and click
    Paste
    .
  5. In the
    Paste hierarchy component
    dialog box, click
    Paste
    .
    Paste Hierarchy Component
    The "
    Component pasted under component successfully
    " message is displayed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal