Site level: Configure Measurands
The Measurands are automatically populated for each site and user cannot add a new Measurand. The user can edit the unit and decimal places for the Measurands.
Edit Measurands
Perform the following steps to edit the measurand:
- Under any site, click theConfigurationmenu and go to theMeasurandstab.MeasurandsThe user can view all the available measurands in the Measurands tab.
- On the required resource type, click the [
] icon.
- In theEdit Measurand Configurationdialog box, edit the fields and clickSave.Edit Measurand ConfigurationThe "Resource type updated successfully” message is displayed.NOTE:Measurand details are auto populated based on the Resource types. Users cannot add or delete the parameters.
Provide Feedback