Remove Component

Perform the following steps to remove the component from the hierarchy list:
  1. Select the required component.
  2. Click the [] icon and click
    Remove
    .
  3. In the
    Remove hierarchy component
    dialog box, click
    Remove
    .
    Remove Hierarchy Component Dialog
TheĀ "
Component removed from hierarchy successfully
" message is displayed.
NOTE:
The user cannot remove the parent component directly. The user needs to remove the child component first and then the user can remove the parent component from the hierarchy list.
If the user removes the parent component directly, the following notification message is displayed:
Remove Hierarchy Component
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal