Site level: Configure Parameters

The Parameters are automatically populated depending on the configured Resource types. Users cannot add new parameters manually and only edit is allowed.
Edit Parameters
Perform the following steps to edit the parameters:
  1. Under any site, go to
    Configuration
    menu, and then to the
    Parameters
    tab.
    Parameters
    The user can view all the available parameters in the Parameters tab.
  2. On the required resource type, click the [] icon.
  3. In the
    Edit Parameters Configuration
    dialog box, edit the fields and click
    Save
    .
    Edit Parameter Configuration
    The "
    Resource type updated successfully
    ” message is displayed.
    NOTE:
    Parameter details are auto populated based on the Resource types. Users cannot add or delete the parameters.
    Users are allowed to edit only the Parameter value.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal