Stop a schedule manually

If you started the Disaster Recovery schedule with the
Run Now
button, and the schedule was inactive, you can stop it with the
Stop
button.
Prerequisites
  • To stop schedules, you must have
    Command a schedule
    permission.
  • To deactivate schedules, you must have
    Edit a schedule
    and
    Command a schedule
    permission.
To manually stop a schedule
  1. Select
    View > Schedules
    , or click the
    Schedules
    button.
  2. Select the schedule to stop.
  3. Click SchedulesStop.
    TIP:
    If the schedule that you started manually was active, the stop button will not be available. In that case, stop the schedule by deactivating it.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal