Deactivate a schedule
If the schedule started on its scheduled time, stop the schedule by deactivating it.
Prerequisites
- To stop schedules, you must haveCommand a schedulepermission.
- To deactivate schedules, you must haveEdit a scheduleandCommand a schedulepermission.
To deactivate a schedule
- SelectView > Schedules, or click theSchedulesbutton.
- Next to the schedule you want to deactivate, clear theActivecheckbox. The schedule will no longer run at its next scheduled run time.
Once you deactivate the schedule, it will begin shutting down. The schedule status will not appear as Disabled until the schedule is completely shut down.
Provide Feedback