Change the appearance of a trend chart
The data on a trend chart represents the data in the system. The appearance of a trend chart and its data may also represent the system. For example, if a bottling line is blue, the data for that line may be configured to appear blue in the trend chart.
Change the appearance of a trend chart to customize the trend chart.
Provide Feedback