Change the background color of a trend chart

Change the background color of a trend chart to change the fill color behind the traces. The default background color for the
Trend Chart
graphic element is white.
To change the background color of a trend chart
  1. Select the trend chart on the screen.
  2. In the
    Properties
    window, select the
    Properties
    tab.
  3. Expand the
    Appearance
    category.
  4. In the
    FillColor
    box, select any color. Select any color in the
    Color Picker
    or a Hex color value entered manually. The Hex value must be in the format #RRGGBB. R, G, and B are Hex digits from 0 through F and represent the color channel values for red, green, and blue. For example, #ffff00 produces yellow.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal