Change the appearance of a trend chart border

Change the border of a trend chart to customize the trend chart to appear on the HMI device. Specify the color, style, and width of the border.
To change the appearance of a trend chart border
  1. Select the trend chart on the screen.
  2. In the
    Properties
    window, select the
    Properties
    tab.
  3. Expand the
    Appearance
    and
    Border
    categories.
  4. In the
    Color
    box, select any color using the
    Color Picker
    or enter a Hex color value manually.
    TIP:
    Hex values must be in #RRGGBB format. R, G, and B are Hex digits from 0 through F and represent the color channel values for red, green, and blue. For example, #ffff00 produces yellow.
  5. In the
    Style
    box, select a style for the border:
    • Line.
      None, Solid, Dash, Dot, Dash Dot, or Dash Dot Dot
    • Cap.
      Flat, Round, or Square
    • Join.
      Miter, Bevel, or Round
  6. In the
    Width
    box, select the width of the border or select
    None
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal