Prevent interaction with a trend chart
Pause

Resume

Pan Forward

Pan Back

To prevent interaction with a trend chart
- Select the trend chart on the screen.
- In thePropertieswindow, select thePropertiestab.
- Expand theAppearancecategory.
- Clear theShowButtonsbox to hide the buttons on the trend chart on the HMI device. Select the box to show the buttons.TIP:Tips:
- Clearing theShowButtonsbox does not depict any changes inView Designer. The buttons do not show on the HMI device.
- To have the trend chart not accept touch or key input even when buttons show on the trend chart, clear theEnablebox.
Provide Feedback