Specify the grid lines on a trend chart
Hide or show grid lines to customize the appearance of a trend chart. By default, horizontal grid lines appear on a trend chart while vertical grid lines do not. Hiding the grid lines shows only the background color of the trend chart behind the traces.
To specify the grid lines on a trend chart
- Select the trend chart on the screen.
- In thePropertieswindow, select thePropertiestab.
- Expand theAppearancecategory.
- Select theShowGridVerticalbox to show the vertical lines on the grid of the trend chart. Clear this box to hide the vertical lines.
- Clear theShowGridHorizontalbox to hide the horizontal lines on the grid of the trend chart. Select this box to show the horizontal lines.
Provide Feedback