Change the appearance of a trace

Change the line color and line width of a trace. Each trace has a solid line by default that is one point wide and has a unique color.
To change the appearance of a trace
  1. Select the trend chart on the screen.
  2. In the
    Properties
    window, select the
    Traces
    tab.
  3. Expand the
    Trace
    card and the
    Appearance
    category.
  4. In the
    Color
    box, select any color using the
    Color Picker
    or enter a Hex color value manually. The Hex value must be in the format #RRGGBB. R, G, and B are Hex digits from 0 through F and represent the color channel values for red, green, and blue. For example, #ffff00 produces yellow.
  5. In the
    Width
    box, select the width for the trace:
    • 1/2
    • 1
    • 2
    • 3
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal