Change the color of text on a trend chart

Change the color of text on a trend chart to change the color of the labels on both axes. Do this to customize the appearance of the trend chart to make the data and time labels easier to read.
To change the color of text on a trend chart
  1. Select the trend chart on the screen.
  2. In the
    Properties
    window, select the
    Properties
    tab.
  3. Expand the
    Appearance
    category.
  4. In the
    FontColor
    box, select a color. Select any color in the
    Color Picker
    or a Hex color value entered manually. The Hex value must be in the format #RRGGBB. R, G, and B are Hex digits from 0 through F and represent the color channel values for red, green, and blue. For example, #ffff00 produces yellow.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal