Change the color of the grid on a trend chart
Change the color of the grid to customize the appearance of a trend chart.
To change the color of the grid on a trend chart
- Select the trend chart on the screen.
- In thePropertieswindow, select thePropertiestab.
- Expand theAppearancecategory.
- In theGridColorbox, In theColorbox, select any color using theColor Pickeror enter a Hex color value manually. The Hex value must be in the format #RRGGBB. R, G, and B are Hex digits from 0 through F and represent the color channel values for red, green, and blue. For example, #ffff00 produces yellow.
Provide Feedback