Create a ramp button
At runtime the operator can use the ramp button to increase or decrease the value of a tag. Ramp buttons can be set up to change a value by either an integer or floating point value. You can use two ramp buttons together to create an increase/decrease control.
To create a ramp button:
- InFactoryTalk View Studio, in theGraphicseditor, selectObjects>Push Button>Ramp, or click the ramp button icon in the toolbox.
- Drag the mouse to position and draw a rectangle the general size and location you intend the button to be.
- In theRamp Button Propertiesdialog box, specify the how the button looks, its tags, and whether to use auto repeat.TIP:Set up a numeric display object to display the value of the ramp button’s Value connection.
Provide Feedback