Ramp Button Properties - Timing tab

The following table shows the options of the
Timing
tab of
Ramp Button
Properties.
Options
Description
Auto repeat rate
Select the number of times per second a button press is registered when the button goes into auto repeat mode. Select 0 if you do not want to use auto repeat.
Auto repeat delay
Select the length of time the button has to be pressed and held down before auto repeat starts.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal