Set up auto repeat for a ramp button

If you set up auto repeat, when the operator presses and holds down the button, repeated button presses are registered until the operator releases the button. For each button press, the application sends the new value to the data source.
If the ramp button is in auto repeat mode, the application ramps the value that was previously sent to the Value connection, rather than reading the value from the data source and ramping the current value. This means that external changes to the Value connection are not recognized while the button is in auto repeat mode.
To set up auto repeat:
  1. In the Graphics editor, in a display, double-click the object to open the
    Properties
    dialog box.
  2. Click the
    Timing
    tab.
  3. Specify the auto repeat settings to use with the button.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal