Data source
The data source can be memory or a device such as a programmable logic controller or an OPC server. The application writes values to, and reads values from, the data source.
The data source is configured to exchange information (in the form of numeric or string values) between the application and the physical machine that the application is controlling.
Provide Feedback