Ramp Button Properties - Connections tab

The following table shows the options in the
Connections
tab of
Ramp Button Properties.
Options
Description
Value
Assign a tag to the Value connection. When the value of the tag changes, the ramp button's action occurs.
Limit
Use this connection with the
Use variable upper/lower limit
check box (on the
General
tab), to create a variable upper or lower ramp limit. Assign a tag, tag parameter (for example #1), expression, or constant, to the Limit connection that will provide the variable value for the limit. In the General tab, the Use variable upper/lower limit check box must be selected.
Ramp
Use this connection with the
Use variable ramp
check box (on the
General
tab), to create a variable ramp value. Assign a tag, tag parameter (for example #1), expression, or constant, to the Ramp connection that will provide the variable value for the ramp. In the General tab, the
Use variable ramp
check box must be selected.
The following table shows other options in the
Connections
tab.
Options
Description
Name
This column shows the name of the connection.
Value update direction
This column shows an arrow to indicate which way data can flow between the connection and the data source.
Right arrow symbol.png tag or expression updates the data source (write connection)
Left arrow symbol.png data source updates the tag or expression (read connection)
Double arrow tag or expression updates the data source and data source updates the tag or expression (read-write connection)
Tag/Expression
Type the tag name or expression associated with the connection. If a tag or expression has already been selected, it is displayed here.
Tag button (...)
Click this button to open the Tag Browser and choose a tag instead of typing the tag name in the Tag/Expression column.
Exprn button (...)
Click this button to open the Expression editor and create an expression instead of typing the expression in the Tag/Expression column.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal