Set up connections for a ramp button

Use the
Connections
tab to set up connections.
To set up connections:
  1. In the Graphics editor, in a display, double-click the object to open the
    Properties
    dialog box.
  2. Click the
    Connections
    tab.
  3. Assign a tag or expression to each connection.
TIP:
If the ramp value is floating point and the Value connection is an integer tag, the application rounds the value before writing it to the tag.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal