Set up a caption and image for a ramp button
Use the
Label
tab to set up a caption or image for a ramp button.To set up a caption or image for a ramp button:
- In a display, double-click the object to openRamp Button Propertiesdialog box.
- Click theLabeltab.
- Specify these properties for the ramp button:
- caption, if any
- image, if any
Provide Feedback