Create a button
The
Button
push button is a generic button that you can set up to run FactoryTalk View SE commands on the press, repeated press, or release actions, or all three. Alternatively, you can set it up to set a tag from 1 to 0 (zero) or from 0 to 1.
TIP:
Buttons support visibility, color, horizontal and vertical slider, horizontal and vertical position, width, and height animation.
To create a Button object:
- InFactoryTalk View Studio, in theGraphicseditor, selectObjects>Push Button>Button.
- Drag the mouse to draw and position a rectangle the general size and place the button is to be.
- In theButton Propertiesdialog box, specify the button style and runtime behavior, the action to be initiated by the button, and its up and down appearance.
- ClickOKto save the settings when you have completed setting up the button.
Provide Feedback