Configure the up appearance of a button

In the
Up Appearance
tab of the
Button Properties
dialog box, specify what the button will look like when it is not in its pressed position.
To configure general properties of a Button:
  1. In the
    Button Properties
    dialog box, in the
    Up Appearance
    tab, specify the fields to describe how the button will look in the Up position, at runtime.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal