Configure the disabled appearance of a Button
In the
Disabled Appearance
tab of the Button Properties
dialog box, specify what the button will look like when it is in its disabled position.To configure the disabled appearance of a Button:
- In theButton Propertiesdialog box, in theDisabled Appearancetab, select theShow Disabled Statecheck box.
- Specify the fields to describe how the button will look in theDisabledposition at runtime.
- When you finish, clickOK.
Provide Feedback