Configure the down appearance of a button
In the
Down Appearance
tab of the Button Properties
dialog box, specify what the button will look like when it is in its pressed position.To configure general properties of a Button:
- In theButton Propertiesdialog box, in theDown Appearancetab, clear theSame as Up Appearancecheck box.
- Specify the fields to describe how the button will look in theDownposition at runtime.
Provide Feedback