Devices
Devices are the modules, drives, controllers, HMI panels, computers, CIP Proxy devices,
OPC UA
servers, and OPC UA
clients that work together to create a FactoryTalk
system.
TIP:
Add devices that share security requirements and that should trust each other to a zone. A device can have one or more ports that are added to the policy model. Connect devices to other devices or zones with conduits.
Provide Feedback