Duplicate a device
Copy and paste a device to duplicate the device with its properties.
- From the navigation bar, either:
- SelectCanvas.
- SelectZonesand then select a zone.
- SelectDevices.
- Right-click a device and selectCopy.
- Right-click blank space and selectPaste.TIP: You can paste the device to the same zone, a different zone, or to the list of unassigned devices. Switching betweenCanvas,Zones, andDevicesdoes not discard the copied device.
Provide Feedback