Replace a device

Replace a device if a device that was configured has failed or must be rotated out for maintenance.
TIP: Device replacement enables the identity and the security configuration of the previous device to be assigned to the replacement device.
  1. From the navigation bar, either:
    • Select
      Canvas
      .
    • Select
      Zones
      and then select a zone.
    • Select
      Devices
      .
  2. Right-click the device to replace and select
    Replace Device
    .
    TIP: In
    Zones
    or
    Devices
    , you can also select the device to replace and then select
    Replace Device
    from the toolbar.
  3. In
    Deploy Configuration to Replace Device
    select when to reset the communication ports on the device:
    • To reset the ports automatically as part of the replacement process, select
      During policy deployment
      .
    • To reset the ports manually at a later time, select
      After deployment
      . The security policy is not being enforced on the device until the ports are reset.
  4. Deploy the policy model to apply the security policies to the replaced device.
    For more information, see Policy model validation and deployment.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal