Edit a device

Edit the device properties to change the device information, security options, or zone assignment.
TIP: You can edit the zone assignment of a device by dragging and dropping the device in
Canvas
. See Move a device.
  1. From the navigation bar, either:
    • Select
      Canvas
      and then select a device.
    • Select
      Zones
      and then select a zone and a device.
    • Select
      Devices
      and then select a device.
  2. In
    PROPERTIES
    , edit the device properties and ports properties.
    For more information, see Device properties and Ports.
Deploy the policy model to apply the changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal