Move a device
You can move devices in the
Canvas
policy model visualization and in the Graphical Explorer
tree.
TIP:
You can also move a device by editing the device properties. See Edit a device.
- From the navigation bar, either:
- SelectCanvas.
- SelectZonesand then select a zone.
- SelectDevices.
- Right-click a device and selectCut.
- Right-click the blank space and selectPaste.TIP:You can paste the device to a different zone or to the list of unassigned devices. Switching betweenCanvas,Zones, andDevicesdoes not discard the copied device.InCanvas, you can drag devices between containers. You can also drop devices from theGraphical Explorertree to theCanvaspolicy model visualization or in the opposite way.IMPORTANT: InCanvas, when you move a device from theOnboarding Areato aZoneor to theUnassignedcontainer, the device cannot be moved to theOnboarding Areacontainer again.
The device is moved to another zone. The
OPC UA
client and OPC UA
server pair moves together.Provide Feedback