Remove the security policy from a device

If you deployed the policy model and the device communications were reset, the device is constrained by the security policy.
IMPORTANT: Even if you uninstall
FactoryTalk Policy Manager
and
FactoryTalk System Services
, the security policy configured for the device is still in effect.
  1. From the navigation bar, either:
    • Select
      Canvas
      and then select a device.
    • Select
      Zones
      and then select a zone and a device.
    • Select
      Devices
      and then select a device.
  2. Unassign the device from a secure zone or delete the device:
    • In
      Properties
      , on the
      Port
      tabs, in
      Zone
      , choose either
      Unassigned
      or a zone that is not
      CIP Security
      or
      OPC UA security policy
      enabled.
    • Right-click the device and select
      Delete
      . Select
      DELETE
      in the confirmation dialog.
  3. Deploy the policy model and select to reset the communications channels during deployment.
    For more information, see Policy model validation and deployment.
The device security configuration is reset to none.
Remove the device from the model or reconfigure the device.
TIP: You can remove the security policy from the device by deleting the device from the security policy model. The changes take place during the next deployment.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal