- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Text vertical alignment
Indicates where the text is positioned on the vertical axis
- BrowseName
- TextVerticalAlignment
Values
Value | DisplayName | Description |
---|---|---|
0 | Top aligned | Text is aligned to the top |
1 | Center aligned | Text is centered |
2 | Bottom aligned | Text is aligned to the bottom |
Provide Feedback