Develop an animated side menu
Use value change animation to smoothly show and hide a side menu.
NOTE:
Download a sample project:
AnimateSideMenu.zip.Side menu example

Prerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.

Select
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a target device.
Run
Provide Feedback