Develop a UI that generates a PDF report

Generate a PDF report with a custom header and footer that contains information from a data grid.
Application example
PDF report example
You can download the report from: Report.pdf
NOTE:
Download a sample project:
PDFReportWithDataGrid.zip
Prerequisites
Application design
Report design
Select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a target device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal