FactoryTalk Optix Studio interface

Following is an example of
FactoryTalk Optix Studio
at design time.
FactoryTalk Optix Studio components
Interface items
Item
Name
Description
1
Commands that apply to all portions of the user interface.
2
Project information model that displays the content and structure of the project in nodes. A node can be a parent that has child nodes.
3
Object types and variable types on which instances of objects are based. Predefined types are grouped in folders according to their purpose. Custom types are grouped in folders that reflect the structure in
Project view
.
4
Messages related to the operation of the
FactoryTalk Optix Application
. Applications that are running and are connected to
FactoryTalk Optix Studio
appear on
Emulator Output
. Project search results.
5
Tabs
Tabs of open objects being modified in the editor. If you hover over a tab to select without saving the project, you are prompted to save your changes.
6
Editor toolbar
Commands that apply to the object type being modified in the editor.
7
Graphic editor for objects. Each editor opens in a new tab and is used for graphic objects and object types, such as tag importers and recipes.
8
Properties to set for the selected node in
Project view
or in the object editor.
9
Events pane
Methods with events generated by the currently selected node. See Events.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal