Export a project

Export a project to archive the project or to send the project to another user in a single file. You can protect the exported project with a password.
  1. In the main toolbar, select the drop down next to
    Save
    .
  2. Select
    Export
    Project to file...
    .
  3. (optional) Change the project name.
  4. (optional) Change the location where to export the project.
  5. (optional) Enter a password to protect the exported project.
  6. Select
    Export
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal