Develop a combo box to pick styles

Create a combo box to choose different application styles. Select a style from the combo box to change the application style at runtime.
Application example
NOTE:
Download a sample project:
StylePicker.zip
Prerequisites
  1. To develop the project
  2. (optional) Add more graphic objects.
    For example, add a button and a label. For more information, see Graphic objects.
  3. Arrange the interface elements.
  4. Save the project.
Application design example
Select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a target device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal