Motion Move Instructions
Use the Motion Move instructions to control axis position.
Available Instructions
Ladder Diagram and Structured Text
IMPORTANT:
Tags used for the motion control attribute of instructions should only be used once. Re-use of the motion control tag in other instructions can cause unintended operation. This may result in damage to equipment or personal injury.
The Motion Move instructions are:
If you want to | Use this instruction |
|---|---|
Stop any motion process on an axis. | MAS |
Home or define an absolute position of an axis. | MAH |
Jog or move an axis at a constant speed. | MAJ |
Move an axis to a specific position. | MAM |
Start electronic gearing between two axes. | MAG |
Change the speed, acceleration rate, or deceleration rate of a
move or a jog profile. | MCD |
Change the command or actual position of an axis. | MRP |
Provide Feedback