Motion Axis Move (MAM)
Use the Motion Axis Move (MAM) instruction to move an axis to a specified
position.
This is a transitional instruction. Follow these steps when using it:
- In ladder logic, insert an instruction to toggle the rung-condition-in from false to true each time the instruction should execute.
- In a Structured Text routine, insert a condition for the instruction to cause it to execute only on a transition.
Available Languages
Ladder Diagram

Structured Text
MAM(Axis, MotionControl, MoveType, Position, Speed, SpeedUnits, AccelRate,
AccelUnits, DecelRate, DecelUnits, Profile, AccelJerk, DecelJerk, JerkUnits, Merge,
MergeSpeed, LockPosition, LockDirection, EventDistance, CalculatedData);
Operands
Ladder Diagram
Operand | Type | Format | Description | ||
|---|---|---|---|---|---|
Axis | AXIS | Tag | Name of the axis. | ||
Motion Control | MOTION_ INSTRUCTION | Tag | Control tag for the instruction. | ||
Move type | DINT | Immediate or Tag | To | Use This Move Type | And Enter |
Move an axis to an absolute position | Absolute | 0 | |||
Move an axis a specified distance from where it is now | Incremental | 1 | |||
Move a Rotary axis to an absolute position in the
shortest | Rotary Shortest Path | 2 | |||
Move a Rotary axis to an absolute position in the positive
direction regardless of its current position | Rotary Positive | 3 | |||
Move a Rotary axis to an absolute position in the negative
direction regardless of its current position | Rotary Negative | 4 | |||
Offset the leader value of a position cam to an absolute
position | Absolute Leader Offset | 5 | |||
Offset the leader value of a position cam by an incremental
distance | Incremental Leader Offset | 6 | |||
See Choose a Move Type for a Rotary Axis below for more
information about rotary moves. | |||||
Position | REAL | Immediate or Tag | Absolute position or incremental distance for the move | ||
For This Move Type | Enter This Position Value | ||||
Absolute | Position to Move to | ||||
Incremental | Distance to Move | ||||
Rotary Shortest Path | Position to move to. Enter a positive value that is less than the
Position Unwind value. | ||||
Rotary Positive | |||||
Rotary Negative | |||||
Absolute Leader Offset | Absolute Offset Position | ||||
Incremental Leader Offset | Incremental Offset Distance | ||||
Speed | REAL | Immediate or Tag | Speed to move the axis in Speed Units | ||
Speed Units | DINT | Immediate | Which units do you want to use for the Speed? Units per sec (0) % of Maximum (1) Time (3) Units per LeaderUnit (4) Leader Units (7) | ||
Accel Rate | REAL | Immediate or Tag | Acceleration rate of the axis in Accel Units | ||
Accel Units | DINT | Immediate | Which units do you want to use for the Accel Rate? Units per sec 2 (0)% of Maximum (1) Time (3) Units per LeaderUnit 2 (4)Leader Units (7) | ||
Decel Rate | REAL | Immediate or Tag | Deceleration rate of the axis in Deceleration Units. | ||
Decel Units | DINT | Immediate | Which units do you want to use for the Decel Rate? Units per sec 2 (0)% of Maximum (1) Time (3) Units per LeaderUnit 2 (4)Leader Units (7) | ||
Profile | DINT | Immediate | Select the velocity profile to run for the move:
| ||
Accel Jerk | REAL | Immediate or Tag | The instruction only uses the jerk operands if the Profile is
S-curve. You must always fill them in however.
Use these values to get started.
You can also enter the jerk rates in these Jerk Units.
| ||
Decel Jerk | REAL | Immediate or Tag | |||
Jerk Units | DINT | Immediate | |||
Merge | DINT | Immediate | Do you want to turn all current axis motion into a pure move
governed by this instruction regardless of the motion
instructions currently in process?
| ||
Merge Speed | DINT | Immediate | If Merge is Enabled, which speed do you want to move at?
| ||
Lock Position | REAL | Immediate or Tag | Position on the Leader Axis where a Follower should start
following the leader after the move has been initiated on the
Follower Axis. See the Structure section below for more information. | ||
Lock Direction | SINT, INT or DINT | Immediate | Specifies the conditions when the Lock Position should be
used. Valid Values = 0-4 Default = None (Enumeration 1-4 are currently not allowed in Time Driven or Time
Based modes.) See the Structure section below for more information. | ||
Event Distance | REAL ARRAY or 0 | Array Tag | The position(s) on a move measured from the end of the move. See the Structure section below for more information. | ||
Calculated Data | REAL ARRAY or 0 | Array Tag | Leader Distance(s) (or time) needed from the beginning of the
move to the Event Distance point. See the Structure section below for more information. | ||
Structured Text
This Operand | Has These Options Which You | |
|---|---|---|
Enter as Text | Or Enter as a Number | |
SpeedUnits | unitspersec %ofmaximum time unitsperleaderunit leaderunits | 0 1 3 4 7 |
AccelUnits | unitspersec 2 %ofmaximum time unitsperleaderunit 2 leaderunits | 0 1 3 4 7 |
DecelUnits | unitspersec 2 %ofmaximum time unitsperleaderunit 2 leaderunits | 0 1 3 4 7 |
Profile | trapezoidal scurve | 0 1 |
JerkUnits | unitspersec 3 %ofmaximum %oftime time unitsperleaderunit 3 %oftime-leaderdriven leaderunits | 0 1 2 3 4 6 7 |
Merge | disabled enabled | 0 1 |
MergeSpeed | programmed current | 0 1 |
Lock Position | No enumeration | Immediate, Real, or Tag |
Lock Direction | None immediateforwardonly immediatereverseonly positionforward positionreverse | 0 1 2 3 4 |
Event Distance | No enumeration | Array or 0 |
Calculated Data | No enumeration | Array or 0 |
For more information on the syntax of expressions within structured text, see Structured Text Syntax.
MOTION_INSTRUCTION Data Type
To See If | Check If This Bit Is Set To | Data Type | Notes |
|---|---|---|---|
A false-to-true transition caused the instruction to execute | EN | BOOL | The EN bit stays set until the process is complete and the rung
goes false. |
The move was successfully initiated | DN | BOOL | |
An error happened | ER | BOOL | |
The axis is moving to the end Position | IP | BOOL | Any of these actions stop this move and clear the IP bit:
|
The axis is at the end Position | PC | BOOL |
|
Description
The MAM instruction moves an axis to either a specified absolute position or by a
specified incremental distance. The MAM instruction can also produce other special
types of moves.
Trapezoidal Move Starting from Standstill

Programming Guidelines
IMPORTANT:
Risk of Velocity and/or End Position
Overshoot
If you change move parameters dynamically by any method, that is by changing move
dynamics [Motion Change Dynamics (MCD)] instruction or by starting a new
instruction before the last one has completed, be aware of the risk of velocity
and/or end position overshoot.
A Trapezoidal velocity profile can
overshoot if maximum deceleration is decreased while the move is decelerating or
is close to the deceleration point.
An S-curve velocity profile can
overshoot if:
- maximum deceleration is decreased while the move is decelerating or close to the deceleration point; or
- maximum acceleration jerk is decreased and the axis is accelerating. Keep in mind, however, that jerk can be changed indirectly if it is specified in % of time.
Guideline | Details | |||
|---|---|---|---|---|
In ladder diagram, toggle the rung condition each time you want
to execute the instruction. | This is a transitional instruction. In ladder diagram, toggle the rung-condition-in from cleared to
set each time you want to execute the instruction. | |||
In structured text, condition the instruction so that it only
executes on a transition | In structured text, instructions execute each time they are
scanned. Condition the instruction so that it only executes on a
transition. Use the structured text construct. For more information, see Structured Text
Syntax. | |||
For a Leader Offset move, enter the follower axis but use leader
units. | Use an Absolute or Incremental Leader Offset move to off set the
leader value of a position cam without actually changing the
position of the leader axis. This shifts the position cam
profile along the leader axis.
The instruction adds in the offset at the Speed, Acceleration,
Deceleration, and Jerk values. | |||
Use % of Time for the easiest programming and tuning of jerk | For an easy way to program and tune jerk, enter it as a % of the
acceleration or deceleration time. | |||
Use Merge to cancel the motion of other instructions | How you want to handle any motion that’s already in process? | |||
If you want to | And you want to | Then set | ||
Add the move to any motion already in process | ![]() | Merge = Disabled Merge Speed = Programmed The instruction ignores Merge Speed but you must fill it in
anyway. | ||
End the motion from other instructions and just jog | Move at the Speed that you set in this instruction | Merge = Enabled Merge Speed = Programmed | ||
Move at the speed that the axis is already moving | Merge = Enabled Merge Speed = Current The instruction ignores the value that you put in the Speed
operand. | |||
Is This an Absolute or Incremental Leader Offset Move? If this is an Absolute or Incremental Leader Offset move and
Merge is Enabled, then the following is true.
| ||||
Use a second MAM instruction to change one that is already in
process. | You can change the position, speed, acceleration, or
deceleration. The change immediately takes effect. | |||
To Change the Position of An | Set Up a Second MAM Instruction Like
This | |||
Absolute Move | Either:
In either case, the axis moves to the new position without
stopping at the old position—including any required change of
direction. | |||
Incremental Move | Either:
| |||
Combine a move with gearing for complex profiles and
synchronization. | You can use a Motion Axis Gear (MAG) instruction together with an
MAM instruction. This superimposes the gearing on top of the
move or the move on top of the gearing. Example: Superimpose an incremental move on top of
electronic gearing for phase advance and retard control. | |||
Choose a Move Type for a Rotary Axis
Move Type | Example | Description |
|---|---|---|
Absolute | Absolute move to 225°. The direction depends on the starting
position of the axis. ![]() | With an Absolute move, the direction of travel depends on the
current position of the axis and is not necessarily the shortest
path to the end position. Starting positions less than the end
position result in motion in the positive direction, while
starting positions greater than the end position result in
motion in the negative direction. The specified position is interpreted trigonometrically and can
be positive or negative. It can also be greater than the
Position Unwind value. Negative position values are equivalent
to their corresponding positive values and are useful when
rotating the axis through 0. For example, –90° is the same as
+270°. When the position is greater than or equal to the
Position Unwind value, the axis moves through more than one
revolution before stopping at an absolute position. |
Incremental | The specified distance is interpreted trigonometrically and can
be positive or negative. It can also be greater than the
Position Unwind value. When the distance is greater than the
Position Unwind value, the axis moves through more than one
revolution before stopping. | |
Rotary Shortest Path | Rotary Shortest Path move from 30° to 225°. ![]() | Important : Only use a Rotary Shortest Path move if the
Positioning Mode of the axis is Rotary (Rotary axis).A Rotary Shortest Path move is a special type of absolute move
for a Rotary axes. The axis moves:
With a Rotary Shortest Path move, you:
|
Rotary Positive | Rotary Positive move from 315° to 225°. ![]() | Important : Only use a Rotary Positive move while the axis
is standing still and not moving. Otherwise the axis could move
in the wrong direction.A Rotary Positive move is a special type of absolute move for a
Rotary axis. The axis:
You can’t move the axis more than one revolution with a single
Rotary Shortest Path move. |
Rotary Negative | Rotary Negative move from 45° to 225°. ![]() | Important : Only use a Rotary Shortest Path move if
A Rotary Negative move is a special type of absolute move for a
Rotary axis. The axis:
You cannot move the axis more than one revolution with a single
Rotary Shortest Path move. |
When MAM (Merge = Enabled) is used on any axis associated with a coordinate system
and a coordinated motion instruction is running on it, Coordinate system’s maximum
deceleration is used to stop remaining axes. If the coordinate system contains
orientation axes, Coordinate system’s Orientation maximum deceleration is used for
stopping remaining Rx, Ry or Rz axes.
Affected Math Status Flags
No
Major/Minor Faults
None specific to this instruction. A major fault can occur if an uninitialized
reference or a reference of incorrect type is passed to the Axis Operand. See Common Attributes for operand-related faults.
Ladder Diagram
Condition/State | Action Taken |
|---|---|
Prescan | The .EN, .DN, .ER, and .IP bits are cleared to false. |
Rung-condition-in is false | The .EN bit is cleared to false if the .DN or .ER bit is
true. |
Rung-condition-out is true | The .EN bit is set to true and the instruction executes. |
Postscan | N/A |
Structured Text
Condition/State | Action Taken |
|---|---|
Prescan | See Prescan in the Ladder Diagram table |
Normal execution | See Rung-condition-in is false, followed by rung is true in the
Ladder Diagram table. |
Postscan | See Postscan in the Ladder Diagram table. |
Error Codes
See Motion Error Codes
.ERR for Motion Instructions.
Runtime Error Condition
The follower move must start at rest if Speed Units = Seconds or Leader Units. This
condition may occur when the MAM with Speed = Seconds or Leader Units is started
while another MAM is in progress (merging or replacement mode).
Extended Error Codes
Use Extended Error Codes (EXERR) for more instruction about an error. See Motion Error Codes
.ERR for Motion Instructions.
If ERR is | And EXERR is | Then | |||
|---|---|---|---|---|---|
Cause | Corrective Action | ||||
13 | Varies | An operand is outside its range. | The EXERR is the number of the operand that is out of range. The
first operand is 0. For example, if EXERR = 4, then check the Speed. | ||
EXERR | Operand | ||||
0 | Axis | ||||
1 | Motion Control | ||||
2 | Move Type | ||||
3 | Position | ||||
4 | Speed | ||||
6 | Accel Rate | ||||
8 | Decel Rate | ||||
15 | -1 | The coordinate system has a Maximum Deceleration of 0. | Go to the Properties for the coordinate system axis and set a
Maximum Deceleration. | ||
0 or more | An axis in the coordinate system has a Maximum Deceleration of
0. |
| |||
Changes to Status Bits
Motion Instruction Predefined Data Type Status Bits
See Status Bits for Motion Instructions (MAM and MAJ).
MAM Changes to Single Axis Status Bits
Bit Name | Meaning | |
|---|---|---|
MotionStatus | The motion status bit for your axis. | |
Bit Number | Meaning | |
AccelStatus | 0 | The axis is not accelerating (FALSE state). |
DecelStatus | 1 | The axis is not decelerating (FALSE state). |
MoveStatus | 2 | The axis is not moving (FALSE state). |
JogStatus | 3 | The axis is not jogging (FALSE state). |
GearingStatus | 4 | The axis is not gearing (FALSE state). |
HomingStatus | 5 | The axis is not homing (FALSE state). |
StoppingStatus | 6 | The axis is stopping (TRUE state). |
AxisHomedStatus | 7 | The axis is not homed (FALSE state). |
PositionCamStatus | 8 | The axis is not position camming (FALSE state). |
TimeCamStatus | 9 | The axis is not time camming (FALSE state). |
PositionCamPendingStatus | 10 | The axis does not have a Position Cam Pending (FALSE state). |
TimeCamPendingStatus | 11 | The axis does not have a Time Cam Pending (FALSE state). |
GearingLockStatus | 12 | The axis is not in a Gear Locked condition (FALSE state). |
PositionCamLockStatus | 13 | The axis is not in a Position Cam Locked condition (FALSE
state). |
TimeCamLockStatus | 14 | The axis is not in a Time Cam Locked condition (FALSE state). |
LeaderOffsetMoveStatus | 15 | The axis is offset (TRUE state). |
CoordinatedMotionStatus | 16 | Sets when the MDAC instruction executes (TRUE state). Clears when
the instruction completes (FALSE state). |
TransformStateStatus | 17 | The axis is part of an active transform (TRUE state). |
ControlledByTransformStatus | 18 | The axis is moving because of a transform (TRUE state). |
DirectVelocityControlStatus | 19 | The axis is not under Direct Velocity Control (FALSE state). |
DirectTorqueControlStatus | 20 | The axis is not under Direct Torque Control (FALSE state). |
MoveLockStatus | 22 | The bit is cleared when an MAS or MASD is executed (goes IP). If either the Follower or Leader axis (or both) is paused by
changing its speed to 0, then the MoveLockStatus bit stays set. Leader Driven Mode The bit is set when the Lock Direction request is satisfied. The bit is not used when the enumeration is NONE. For the enumerations Immediate Forward Only and Immediate Reverse
Only, the MamLockStatus bit is set immediately when the MAM is
initiated. For the enumeration Position Forward Only and Position Reverse
Only, the bit is set when the Leader Axis crosses the Leader
Lock Position in the specified direction. The MoveLockStatus bit is cleared when the Leader Axis reverses
direction and the Follower Axis stops following the Leader Axis.
The MoveLockStatus bit is set again when the Follower Axis
resumes following the Leader Axis. Time Driven Mode The bit is not used when the enumeration is NONE. |
JogLockStatus | 24 | The axis is not in a Jog Locked condition (FALSE state). |
MaximumSpeedExceeded | 27 | Sets when the maximum axis speed that is specified in the axis
configuration is exceeded during a move (TRUE state). Clears
when the speed is reduced below the limit (FALSE state). |
Motion Status Bits
If the Move Type Is | And Merge is | Then the Instruction Changes These
Bits | ||
|---|---|---|---|---|
Bit Name | State | Meaning | ||
NOT Absolute Leader Offset or Incremental Leader Offset | Disabled | MoveStatus | TRUE | Axis is Moving. |
Enabled | MoveStatus | TRUE | Axis is Moving. | |
JogStatus | FALSE | Axis is no longer Jogging. | ||
GearingStatus | FALSE | Axis is no longer Gearing. | ||
Absolute Leader Offset or Incremental Leader Offset | ![]() | LeaderOffsetMoveStatus | TRUE | Axis is Offset. |
Example
Ladder Diagram

Provide Feedback