API function reference
The API functions can be categorized into several major groups by functionality. The following table provides a brief description and a link to each group.
API function type | Description |
Defines data items and initialize the data definition table. | |
Converts data from one format to another (between processor data types and application data types). | |
Opens and closes drivers. | |
Reads solicited data items from processors, writes solicited data items to processors, and processes unsolicited data items. | |
Sends packets to processors. | |
Manages communication sessions with network interfaces. | |
Registers and unregisters unsolicited messages. | |
Performs utility operations. |
Provide Feedback