Utility functions
API function | Description | RSLinx Classic | INTERCHANGE |
DTL_CLOCK | Synchronizes clock in an RM with the one in the host. | Not supported | Supported |
DTL_ERROR_F/P/FP | Translates status codes to text string to be placed in a buffer. | Not supported | Supported |
DTL_GET_MODIDS | Gets and displays list describing modules in a PI chassis. | Not supported | Supported |
DTL_PING | Verifies connectivity of Ethernet interfaces. | Not supported | Supported |
DTL_SYNC | Sets date and time of an RM's clock to that of the host. | Not supported | Supported |
Returns structured address associated with specified host solicited data item. | Supported | Supported | |
Provide Feedback