Configuration functions

API function
Description
RSLinx Classic
Interchange
Adds a data item to the data definition table.
Supported
Supported
Returns the number of available openings in the data definition table.
Supported
Supported
DTL_FCREATE
Creates PLC data table file.
Not supported
Supported
DTL_FDELETE
Deletes PLC data table file.
Not supported
Supported
DTL_FSIZE
Returns the number of words or structures in a PLC data table file.
Not supported
Supported
Creates/initializes data definition table.
Supported
Supported
Initializes the data definition table and enables optional DTL features.
Supported
Not Supported
Returns number of bytes needed to store data in the host's format.
Supported
Supported
Returns host data type from a data definition.
Supported
Supported
Uninitializes data definition table.
Supported
Supported
DTL_UNSOL_DEF
Adds unsolicited data item to table.
Not supported
Supported
Deletes a data item from the data definition table.
Supported
Supported
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal