DTL_INIT_EX

The DTL_INT_EX function initializes the RSLinx Classic data definition table and enables optional DTL features based on the bits set in the flags parameter.
DTL_RETVAL DTL_INIT_EX(
table_size, flags
)
UNSIGNED LONG
table_size
;
/* maximum number of data items*/
UNSIGNED LONG
flags
;
/* options for initializing DTL*/
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal